Other Parts Discussed in Thread: BQ27Z561, , EV2400
BQ27Z561's SDA pin become 2V when master access 0x55 address(BQ27Z561 7bit I2C address).
Why does not the SDA pin become 0V?
Pullup resistor is 10kOhm at the SDA pin.
Best Regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
BQ27Z561's SDA pin become 2V when master access 0x55 address(BQ27Z561 7bit I2C address).
Why does not the SDA pin become 0V?
Pullup resistor is 10kOhm at the SDA pin.
Best Regards,
Dear Baldino san
Thank you for your reply.
We use nRF5340 made Nordic Semiconductor.
The nRF5340 is supported for clock stretching (non I2C compliant).
Please refer to the below.

We tried changing from BQ27Z561-R2 to BQ27421 on the same I2C line.
Result, I2C communication is correct from nRF5340.

Is there a difference between BQ27Z561 and BQ27421 in I2C communication?
We returned to BQ27Z561 and connected to the EV2400 on the same I2C line.
Result, I2C communication is correct from Battery Management Studio via the EV2400.

Could the nRF5340 support for clock stretching (non I2C compliant) be the cause of BQ27Z561's SDA pin does not become 0V? (become 2V.)
In that case, how should we use the nRF5340?
Best Regards,
Hello,
The main difference between the I2C communication of the bq27z561 and the bq27421 is the 100kHz rise time value, with bq27z561 being 1000ns and bq27421 being 300ns:
bq27z561:

bq27421:

I believe the issue lies in the structure for the bq27z561 not matching this structure found below due to how these parameters are set:

Regards,
Anthony Baldino
Dear Baldino san
Thank you for your reply.
I found out the cause.
nRF5340 output configuration is CMOS, not Open Drain.
We set the Open Drain.
Please refer to the below.

I2C communication is correct.
Best Regards,