Part Number: LM3643
Hi Sir,
My customer would like to add an external P-MOS to do the LED switch.
Could you please help to review the below schematics and advise comments?
My customer also has some questions as below.
The default condition is the LED light working normally by LM3643 controlled and the test step is as below.
Step 1: Only turn off the Q2, and the LED lights out.
Step 2: turn on the Q2 again.
Is the LED light working normally after step 2?
Do we need to reset the I2C setting after step 2? or concerned about any side effects on the LM3643 (ex: H/W reset, OVP, or other)?
Flash_LED+ voltage = 3V, ILED = 700mA