Hi,
I've been reading the datasheet and I did my schematic for the LMR36502F3RPER, might you tell me if it is ok? the switching frequency is near 600kHz and the output must be 5.1V, considering a Vin(min) = 17V and Vin(nom) = 32.4V. In the next image I used the LMR36502RP5 and I don't know whether there is some difference or not with the LMR36502F3RPER, both seems to be almost the same. I got Vout = 5.1V which is what I want.