Hi,
I have a working boost converter based on the TPS61085 chip,
I want to make some changes so the design will get certified as IS (Intrinsically Safe).
The most important change is limiting the current at the output, and I plan to do that with a resistor (as small as possible) in series with the load, (see picture attached)
the output voltage is set to 12V, and the max current that I will drow is 0.3A,
As the current flow on this resistor, there will be a power drop on it, and the load will get less voltage than I needed,
to overcome this, I wanted to connect the feedback pin after this resistor,

Will this work?
How will the system react to high current changes?
Any other good idea to make the system IS approved?
Thanks
Shamir