Hello Ti Team
We are using BQ76052 AFE for 48volt BMS application.
We are facing issue of voltage fluctuation in the field.
Meaning of voltage Fluctuation means one cell is reading higher value and second corressponding cell is reading Lowe value but the actual value of cell is accurate.
Example :-
Cell 1-10:- 3760
Cell 11:- 3657 Actual Voltage is 3760
Cell 12:- 3966 Actual Voltage is 3760
Cell 13-14 :- 3760
If we can divide cell 11 and cell 12 we will get approx same value with a difference of 30mV to 50mV.
Note :- We have deployed 8000 Battery pack with the same BMS.
Out of 8000 Battery pack we have faced two types of issues on the voltage fluctuation.
Issue 1 :- Voltage Fluctuation will be auto corrected (This type of issue we have seen in 100 Battery pack approx.)
Voltage Fluctuation will be auto corrected means one cell read higher voltage and second corresponding cell will read lower voltage and this issue will be autocorrected.
Issue 2 :- Voltage fluctuation will not be autocorrected (This type of issue we have 70-80 Battery packs approx)
Voltage Fluctuation will not be auto corrected means once the one cell reads higher voltage and second corresponding cell reads lower voltage then this scenario will be continue there.
This scenario can be rectified by two ways
1.Disconnect the sensing wire and again connect then this will be resolved.
2.ON cell balancing for that particular cell then this will be resolved.
We need your support to resolve this issue .or get to know what are the possible cases in which this type of issue occur
Thanks and Regards
Mohit Aggarwal