Other Parts Discussed in Thread: TIDA-01480
I am using the PMIC to power an FPGA.
Due to the large number of decoupling capacitors required on the rail the soft-start current will be above the rating of both the PMIC and the saturation current of the inductor. Please advise whether this is safe and if not how I resolve as even if I replaced the inductor with one with a higher saturation current, the soft-start current would still be ~ 3.5A
I have ~900uF on a 3V3 rail driven by DCDC3.