Other Parts Discussed in Thread: BQ25620,
Hello,
I would like to know if it's possible/recommended to put a diode between IN input and SYS output of BQ25180YBGR.
The purpose on this is so that the system that power the BQ input is a 5V bus that in certain moment could fall. In case of fall, the battery should source both the SYS pin and the 5V bus (in case of the battery sourcing the 5V, this bus will not be expected to have the 5V level, but the battery's - and this is ok).
Regards,
Emanuel.