This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS22950: Can the part's ON pin be driven by 1.8V logic

Part Number: TPS22950


Hi, I am consideringthe device to be driven by 1.8V SOC but it looks ( if I read the data sheet correctly) that there is possibility it will not work correctly .

Typical max Vol=0.2*VCC=0.2*1.8=0.36V while Tavle 7.3 in the data sheet lists Vil =0.35V max . Is it safe to connect the device to such 1V8 logic? Will it function properly. Data sheet does not state if Vil is max accepted low voltage or max voltage for internal pull up enable only?