Other Parts Discussed in Thread: BQ25672, BQSTUDIO, BQ25798, EV2400, BQ25672EVM
Hi Team,
We are using charger bq25672 with fuel gauge bq28Z610 to test single cell battery charge/discharge. The charger bq25672 POR default settings for 1S are ICHG 2A VREG 4.2V and VSYS 3.5V per data sheet SLUSEB9A section 8.3.2 PROG Pin configuration. We like to change ICHG limit to1A instead of 2A. We launch BqStudio and select charger bq25798.bqz file (equivalent to bq25672.bqz), trying to set register REG0x03 ICHG to 1000mA and VREG 4160mV, VSYS 3500mV but register updated did not save when restart the charger ? How can change cell POR default settings and save? Please advise. Thanks