This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5022: LTSpice Simulation Failed

Part Number: LM5022
Other Parts Discussed in Thread: LM5116

Hi Guys,

I am trying to replicate the example circuit in LM5022 datasheet, but the simulation failed every time but I can't see where went wrong. Below are the schematic, error message and error log.

Questionable use of curly braces in "b_abmgate yint 0 v={if(v(a)>{{vthresh}},{{vdd}},{{vss}})}"
Error: undefined symbol in: "if([v](a)>((vthresh)),((vdd)),((vss)))"
co1: Increased Cpar to 4.7e-12
u2:1:dclp: Emission coefficient, N=0.01, too small, limited to 0.1
u2:dclp: Emission coefficient, N=0.01, too small, limited to 0.1
u2:3:d_d1: Emission coefficient, N=0.01, too small, limited to 0.1
Direct Newton iteration failed to find .op point. (Use ".option noopiter" to skip.)
Starting Gmin stepping
Increasing initial diagonal Gmin to 100
Increasing initial diagonal Gmin to 1000
Increasing initial diagonal Gmin to 10000
Increasing initial diagonal Gmin to 100000
Increasing initial diagonal Gmin to 1e+06
Initial Gmin=1e+06 failed
Gmin stepping failed

Starting source stepping with srcstepmethod=0
Source Step = 3.0303%
vernier = 0.25
Source Step = 0.0177557%
Starting source stepping with srcstepmethod=1
Source Step = 3.0303%
vernier = 0.25
Source stepping failed

Pseudo Transient failed in finding the operating point at 40.7099 ms.
Trouble finding operating point....skipping operating point for Transient analysis.
Ignoring empty pin current: Ix(u2:vin)
Ignoring empty pin current: Ix(u2:fb)
Changing Tseed to 1e-07
Changing Tseed to 1e-09
Changing Tseed to 1e-06
Changing Tseed to 1e-10
Changing Tseed to 1e-05
Changing Tseed to 1e-11
Changing Tseed to 0.0001
Changing Tseed to 1e-12
Changing Tseed to 0.001
Changing Tseed to 1e-13
Changing Tseed to 0.01
Changing Tseed to 1e-14
Fatal Error: Analysis: Time step too small; initial timepoint: trouble with node "u2:44"