Other Parts Discussed in Thread: SN65472-EP, DS3668
Hi,
Our application is to provide driving current to the sending optical module of AVAGO. The recommended device in the datasheet is SN75451.
SN75451 can meet RoHS, but the operational temperature (0-70 ℃) does not meet the industrial temperature range.
In the same datasheet, SN55451 can meet the industrial temperature range(-55-125 ℃), but does not meet RoHS.
Please help to find a device whitch is pin to pin compatible and meet both RoHS and industrial temperature(-40-85 ℃ or above).
Regards.