I’m using this component new into my design: TPS1HC100BQPWPRQ1
Previously I was using TPS1H100AQPWPRQ1 which EN pin Vin High was 2V
That’s why Im using a digital switch to provide 3.3V to EN pin. Using 1.8V from SoC to supply IN signal of digital switch (Pin 2 of Q9)
For the new IC Vin High is 1.5V,
Can I get rid of Q9 and connect my SoC directly to EN pin? Do you see a potential risk of not enabling the driver when is needed?