This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS40322EVM-074: TPS40322

Part Number: TPS40322EVM-074


Is it possible to modify the output voltage of the TPS40322EVM-074 to give 2V@18A. The default setup is 1.2V@30A.

I tried using WEBENCH POWER DESIGNER but the tool always produces a single phase design.

Bill