This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24195L: Which direction does BATFET body diode face?

Part Number: BQ24195L
Other Parts Discussed in Thread: BQ24195

Hello,

The block diagram for BQ24195 is not very clear as to which type of MOS the Q4 BATFET is and which direction does its body diode point? Should I expect VSYS to go to 0V when BATFET is disabled?

Thanks and regards,
CraigQ4 BATFET

  • Hi Craig,

    The functional block diagram gives an idea of the device behavior but may not necessarily directly reflect the device internals and how they operate. If the BATFET is disabled, SYS's voltage may depend on VIN presence. If VIN is not present then SYS will be low.

    Best Regards,

    Juan Ospina