Hi team,
What is the difference between the continuous drain current(package limited) and continuous drain current as below? Why the second one is smaller? What is the limit condition?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
What is the difference between the continuous drain current(package limited) and continuous drain current as below? Why the second one is smaller? What is the limit condition?

Hello Hale,
Thanks for the inquiry. Please see the blog at the first link below for more information on MOSFET continuous current ratings. The package limit is related to the internal connections between the silicon die and the plastic package is independent of temperature. The silicon limit and smaller value of continuous current are both calculated numbers. The silicon limit assume TC = 25°C and uses RθJC in the calculation whereas the lower limit assumes TA = 25°C and uses RθJA in the calculation. I'm including a second link to an app note that includes links to all of TI's web based FET technical information including the datasheet series of blogs.
https://e2e.ti.com/blogs_/b/powerhouse/posts/understanding-mosfet-data-sheets-part-3
https://www.ti.com/lit/an/slvafg3b/slvafg3b.pdf
Let me know if you have any questions.
Best Regards,
John Wallace
TI FET Applications