Hello,
I'm using the TPS62745 in several product lines to regulate a 9V battery voltage back to 3.0 volts. Over the past 4 years (from June 2019 onward), several thousand items have been produced and sold, and all tested OK after production.
However, we're increasingly seeing products being returned with defective TPS62745 regulators - 13 so far. The failure mode is usually excessive current draw (15 - 60 mA @ 9V), draining the battery within a day. In about half the cases, the regulator still works, with 3.0 volts output; in the other half, no output voltage is present any more. As far as we can tell, failure occurs instantaneous, without warning.
Replacing the TPS62745 fixed the problem in all cases, but that of course doesn't tell me what caused the failure, or how it might be prevented.
Some more technical details:
- Supply circuit: almost identical to the typical application schematic on datasheet page 1 (4.7 uH inductor, 10 uF input and output capacitor).
- Supply source: 9V battery with a series diode to block reverse polarity, so the actual input voltage will never reach the 10V maximum value of the TPS62745.
- Current draw: 50 mA maximum; in normal operation, some 20 uA is drawn at the 3.0 volt side.
- Possible external overvoltage source: static discharge on switch cable (2.5 meters) - but ESD discharge tests on this cable suggest sufficient ESD immunity (no failures occurred during testing).
- Possible internal overvoltage source: bistable relay, with bidirectional 3.3V TVS diode across the coil. Testing shows no spikes higher than 100 mV, even without the TVS diode.
- Production: reputable PCB house.
So I'm wondering what might be causing the device to sometimes fail. Are there any known causes that I may have overlooked? Or could it be a bad batch of components? I'm checking with the PCB house if the failed devices are all from the same batch - during the big component shortage 2 years ago, batches of dodgy components regularly made it onto the market, and I've had some of those end up in my other products as well. But so far, the failed devices seem to stem from at least 3 completely separate batches, so this doesn't seem likely.
Any ideas are welcome,
Regards,
Richard