Hello, I'm wondering the input current range of LP87745-Q1.
Is the reason TI didn't write it down because the input current changes according to the load current?
Or Is it confidential? If so, I'll create new thread in internal forum.
Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello, I'm wondering the input current range of LP87745-Q1.
Is the reason TI didn't write it down because the input current changes according to the load current?
Or Is it confidential? If so, I'll create new thread in internal forum.
Thank you.
Hello Ian,
Yes It depends on the load current and output voltages. Because output voltages are configurable. It is not confidential information but understandable in the sense that input current figures are variable based on what is configured at the output rails. Also you need to take account of losses as well.
Best regards,
Ishtiaque Panhwar