This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2662: TPS26620DRCR reverse input polarity protection test failed

Part Number: TPS2662


Dear  TI team:

A problem was encountered when testing the input polarity protection function about the Efuse IC TPS26620DRCR

1. Input negative power supply 25V, but power supply display voltage 3.12V, current 1.799A(The limiting current is set to 1.8A), Normally it should be displayed as 25V, 0A, 

Could you please help confirm what the problem is?

2. Below is the schematic, please help to check if there is any problem