Hi,
i want to use this as a ideal diode. Power in on the left ist 10V to 60V. When i got a load above 250uF my MOSFET Q1B burns out when I turn it on. I use Power MOSFETS from Infineon (IPG20N10S4L-22). I also tried vishay (78-SQJB80EP-t1_GE3), same result. I guess i made a mistake with the inrush current limiting?
1. Scematic
In green the Voltage on the Output. In Yellow the current on the Output.
2. Turning on with 60V on Input and 47uF on Output.
2. Turning on with 55V on Input and 380uF on Output.
Unfortunately the current got cut off by my Current clamp meter. After a spike like this the mosfet has a resistance of 5Ohm to 10Ohm between drain and source and can not be switched any more.
Have you any advise of how i can make sure that i can power devices from this output with even greater capacitors to load?