I don't want to use the current sensing feature included in the LM25149 buck which brings up two questions:
1) Can I short ISNS+ to VOUT so that the overcurrent will never trip? Are there unintended consequences of doing that?
2) The equation 35 in the datasheet for the final calculation of the buck inductor includes the value of the sense resistor. This is for internal slope compensation. If I omit the sense resistor(Rs = 0) then this equation no longer works. Can I just use equation 33 and forger about equation 35?
Thank you!