This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS629210: Cyclical Resetting

Part Number: TPS629210


Hello,

We are having an issue where, cyclically, the regulator will stop switching every 150ms for 1.5-4ms, resetting all our electronics. We do not know what is precipitating the pauses in switching.

Our input voltage ranges from 7V down to 3.9V, our output voltage is 3.3V.

As the input voltage reaches 4.15V (roughly, varies a little), the regulator begins a cyclical pause in operation. Every 156ms, switching will halt completely for at least 1.68ms, with additional smaller pauses (presumably as the regulator resets). This resets our electronics.

After this halting behavior, the regulator resumes normal operation, until about 156ms have passed and then it pauses operation again.

The cyclical resets do not stop until the input voltage is raised again to roughly 4.5V.

During all of this, the ‘Power Good’ output will indicate correctly, as shown in this image with the green trace.

Increasing the value of C_out has little to no impact.

Switching C_out to a higher ESR tantalum makes the voltage drop on the output by just about 100mV or so. Problem remains.

Decreasing the value of C_out to 10uF has some small impact to the oscillations that are sometimes present, but the problem remains.

Replacing our implementation with an output from a TPS629210EVM yields the same results, but worse. The resetting behavior starts as early as approaching 5V, instead of 4.15V

The first pause in switching lasts about 1.685ms, then it alternates between the two following states, one with 2 breaks in the switching, and one with 3 breaks in the switching.

Sometimes the 2nd pause has an pulse train.

Sometimes the 3rd break is longer.

Since this behavior is being replicated on both our implementation and the evaluation board, we are thinking this could be some behavior of the regulator we do not understand, or are misinterpreting. Perhaps some aspect of the DCS-Control behavior.

We would greatly appreciate any assistance you can provide us with this.

Thanks for your time.

  • Hi Lucia,

    The schematic looks good.

    1. Could you please share your layout file for review?

    2. Also is it possible you catch the waveform of VIN/EN voltage together with the output voltage in the same window for clear analysis? I think you're catching the SW and VOUT now.

    3. What's the output current during this transition?

    I guess the issue may be related to the poor layout or the current capability of the battery. However, we need more info for further check.

    Thank you so much!

    Athos

  • Hello Athos,

    Thank you for your quick reply, we appreciate it.

    The issue was not with the regulator, we had a misbehaving circuit that was intermittently dropping the input voltage. We have resolved the problem.


    Thanks again for your time, hope you have a great day.