Other Parts Discussed in Thread: BQ25713B, BQ25713, BQ25790, BQ25731
The main board of our product uses TPS25750 and BQ25713B as the power management solution.
When we used the Application Customization Tool to configure the PD controller, we noticed that the battery charger selected for integration in the Battery Charger Configuration field did not include BQ25713B. We try to use the Application Customization Tool to generate firmware that integrates BQ25713 to bring-up the combination of TPS25750 and BQ25713B, but we saw that the BQ component was not successfully initialized.
We later clearly learned that the initialization failure was caused by the difference in the I2C slave addresses of BQ25713 and BQ25713B, so the TPS25750 program could not control BQ25713B.
We would like to know, if can the TPS25750 still be integrated with the BQ25713B, and can it fully control the BQ device? Even if the two can be successfully integrated, can we still use the TPS25750 Application Customization Tool to configure the firmware for the TPS25750?
Thanks.
Wei-Ting