Part Number: TPS563252
Other Parts Discussed in Thread: TPS562242
Hi Expert,
I'm curious if TPS563252/7 EN pin- pull high will happen any risk ? or must be connect the resistor maintain the threshold ?
Eddie
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Eddie,
Thanks for reaching out. The resistor is not a must requriement.
(1) If no EN signal, you can use a top resistor and bottom resistor for EN.

(2) Another way is to have EN signal to control (<5.5V).
Thanks and kindly let us know anything unclear!
BRs
Lucia
Hi Lucia and Expert,
If i do not have EN control and need it , Can i just let the EN pin keep flat ?
Do I see any risk in here ?
Eddie
Hi Eddie,
Could you please clarify "let EN keep flat"? Do you mean floating EN pin?
Thanks!
BR
Lucia
Hi Eddie,
If you mean EN pin floating, it can not enable the device. TPS563252/7 EN default is low which means that if it's floating it will not enabled. TPS562242 (2A) default status is high if you would like to make EN floating.
Thanks!
BRs
Lucia
Hi Eddie,
We have not seen an update from you for one month, so I assume the questions are answered and the issue is solved.
If you don't have any further questions, can you please close the thread by clicking on resolved. Clicking the Resolved Button also helps us to maintain this forum. Thanks!
BRs
Lucia