Hi team,
I found that there are two cases of quiesecent current. How do we calculate the total quiescent current from them? Should I just sum them(IQ_VOUT, IQ_VIN)?

Best regards,
Shunsuke Yamamoto
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
I found that there are two cases of quiesecent current. How do we calculate the total quiescent current from them? Should I just sum them(IQ_VOUT, IQ_VIN)?

Best regards,
Shunsuke Yamamoto
Hi Shunsuke,
Thank you for reaching out.
1. When Vin=2.9V to 5.25V, internal VCC is powered by Vout. At this time, IQ into Vout is 80uA and IQ into Vin is 1.5uA. When Vin=5.5V to 23V, internal VCC is powered by Vin. At this time, IQ into Vin is 80uA and IQ into Vout is 2uA. This is why there are two ranges.
2. Even though internal VCC is power by one of Vin and Vout, there is still some leakage current caused by internal circuit. So the other pin still exist small IQ. This is why both Vin and Vout exist IQ.
3. Would you please explain what does the total quiescent current refer to? Do you mean input current with no load?
Regards,
Mulin