Regarding the IC BQ25895, I'm using this IC to power management which managed by MCU and provide power for Linux board.
I noticed that when I use the battery and connect a 12V input source, the measured VBUS is approximately 11.3 ~11.5V. However, when I disconnect the battery, the power measures around 11.8V. Could someone clarify why this is happening?