Other Parts Discussed in Thread: LM74722-Q1
LM74720-Q1/LM74722-Q1"Programming Overvoltage Threshold and Battery Sensing, according to EVM BOARD R14 and R15, when connected to VIN during shutdown, may result increase in standby current, with the specification requiring standby current(Dark current) to be less than 120K.
1.Is it possible to connect a 1M resistor in series to VIN between BATT_MON to reduce dark current?
2.Is it recommended to connect it to the vehicle's IGN/ACC pin for overvoltage protection detection?"
3.Choose not to use the OVP function and not install the resistor?
4.Choose not to use the OVP function but install resistor