This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM53604: Questions of TPSM53604

Part Number: TPSM53604
Other Parts Discussed in Thread: TPSM53603,

Dear Team,

Can you help us see if our 53603 can be directly replaced by 53604? There is no need to change the peripheral BOM, right?

SCH diagram as below,  please help to check it, thank you very much!

Many Thanks,

Jimmy

  • Hello,

    The TPSM53603 and TPSM53604 are pin-to-pin compatible and can be interchanged. Only difference between the two are current limit trims. 

    There should not be a need to change BOM if the application stays the same. 

    Regards,

    Jimmy