This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25120A: NTC management

Part Number: BQ25120A

Dear Sir or Madam,

We are currently using the BQ25120A in order to manage the charge of our battery. In order to achieve it properly, we'd like to cut the charge when the battery temperature is under or above a certain voltage.

We used the formula given in the datasheet to compute R(Hi) and R(Lo). It worked well when we defined a minimum temperature of 0°C and a maximum temperature of 40°C. But we'd like to set a minimum temperature of 10°C. In this case, the value of R(LO) become negative.

Do you have any explanation about it ?

Have a nice day,

Kind regards,

William.