This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92513:出力(PH)にスナバ回路を接続することによって出力電流にオフセットが発生する

Part Number: TPS92513

出力にスナバ回路を追加することで約20mAのオフセット電流が発生しています。

この説明として以下の内容で間違いないでしょうか。

間違いであれば正しい説明をご教示願います。

<評価回路>

<評価方法>

以下の負荷・入力条件でスナバ回路有無の測定結果を比較し考察

負荷:SMBB760D-1100(USHIO) Vf=2V

IADJ:26.6mV入力

PDIM:3.3V矩形波を36msecワンショットで入力

測定点CH1(イエロー):M9-10pin PH

測定点CH2(シアン):電流プローブ(アノード側)

測定点CH3(マゼンタ):L3負荷側(2次側)

測定点CH4(グリーン):M9-7pin ISENSE

<結論>

③のようにスナバ回路がある方がパルスが分散されていないため、①の結果は低くなるが、1ショットのDuty比が高いので、トータルの電流量②が増加する。

  • Hi Customer,

    Your TI FAE has already contacted me before and I have answered the question to him. He will contact you later.

    I am going to close this thread. Feel free to contact me if you have any further question.

    Best Regards,

    Steven