Other Parts Discussed in Thread: GPCCHEM
Hi
The customer test with BQ40Z50-R1, The IDs 1156 and 1157 calculated by GPCCHEM were used for low temperature compensation respectively, and the verification test was performed according to the compensation file. The effect was not good. At -40 degrees, the CHEM ID of 1156, the RSOC jumped from 10% to 0%; The CHEM ID of 1157, the percentage jumps from 12% to 0%.
The -40c compensation report and GPCCHEM report as below:
3617.temp compensation-report.zip

The -40C log data as below:

The gg file as below:
How to improve this drop issue?
Waiting for your reply.
Thanks
Star