Other Parts Discussed in Thread: TPS65219
Hello,
Into this table extracted from TPS65220 SLVSGY1A – DECEMBER 2022 – REVISED JULY 2023.
I wonder if there is an typo concerning VIL max.
I2C standard define VILmax as 30% of VDD and VIH min as 70% of VDD also.
I guess that into this datasheet VIHmin =1.26V if related to 1.8V*70%=1.26V ....so VIL max= should be 0.54V.
Is it right?
I guess there is a typo because into I2C standard VOLmax is also defined as 0.4V for VDD>2V