This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A39: TPS7A39 Simulation fails to converge when loaded

Part Number: TPS7A39


I have put together a simple bipolar power supply base on the application notes in the TPS7A39 datasheet.

The PSpice simulation works fine as long as the output is unloaded, but I would like to add components to the output to see how it will behave under load.

However, as soon as I add any loading components, the simulation fails to converge.  The attached version of the project includes two resistors, R14 and R15, intended to load the regulator at approximately 70mA. The simulation runs fine without them, but fails to converge as shown.

What am I doing wrong?

bipolarbatterycharger-2023-11-10T17-12.zip