Other Parts Discussed in Thread: BQ25792EVM
Hi,
I've a design with the charger with marking 14A90Z8. When VBUS is applied without the battery connected after 155 ms the REGN turns on at 2V and switches off after additional 85 ms. It does that for 7 times with 500 ms in between and then stops. There is no output on SYS. When I plug in the battery there is output on the SYS and when VBUS is applied the battery doesn't charge and no output on the REGEN. Attached is the schematic and REGN behavior on VBUS only. Battery is 4S and VBUS is 24V but tested from 16V to 23V. Could you please guide me what might be the reason?
By the way, I've seen a thread that there was a faulty series of the bq25672's, could you please also verify that this behavior is not related to that?


Thanks,
Tomasz