Part Number: REF102
Hello Team,
We are planning to use the IC REF102 for a 1mA precise current generation.
The drift of the current source must be below 100nA.
The same current is used as the excitation current of PT1000 and PT100 temperature sensors.
Can we achieve the 100nA precision with the IC?
Initially, we were using a Howland current source, and the drift and the noise from the Howland current pump were very high since it has many components, and all those components contribute to the temperature drift and noise.
Can we achieve the 100nA precision with the IC?
Also, we need a 10uA current as the excitation current of some other sensors like the diode.
The R in the above circuit can be varied using an analog switch.
But the analog switch will also have resistance, so we need to adjust the voltage to the 4th pin of the REF102 to get the correct 1mA or 10uA (We also need calibration to nullify the offset due to aging).
So we are planning to use a DAC to inject a voltage to the 4th pin pf the REF102 IC.
Can you please comment on this?
Is there any good approach other than this to get a precise current source within our tolerance limit?