Other Parts Discussed in Thread: BQ25792
Hello.
I'm using TPS25750 + BQ25792 combo.
I Have USB connected to TPS25750 (VBUS ~5-20V) and I have MCU connected to TPS25750 and performing below operations at startup:
-Patch TPS25750 over I2C (Low Region Binary generated using latest GUI)
-Setup BQ25792 using 4CC: I2Cr and I2Cw commands (i.e set EN_ADC=1, SFET_PRESENT=1, IBAT_EN=1, WATCHDOG=0)
Device is then working normally and as expected until I unplug USB power source (VBUS ~0V), then my settings (ie. SFET_PRESENT=1, IBAT_EN=1) are restored back to Defaults.
When MCU is running, TPS25750 is also always provided with stable 3.3V on VIN_3V3 pin.
Is that normal behaviour and should I always monitor for every USB plug detach and setup BQ25792?
Do we know in which scenarios TPS25750 is sending reset command to BQ25792?
Regards Mateusz Kusmierz