This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3150: The maximum output current for LM3150

Part Number: LM3150


Hi,

We use the LM3150 for our power rail, we know the max. output current for LM3150 is 12A in datasheet, 

we request the LM3150 for below spec.:Input voltage: 16-36V, output 5V/12A, and we find the output current can't reach the 12A max. and only 11A we can regulate,

and the inductance temperature is more than 80℃,

So please kindly review the schematic diagram and provide your comment how to adjust the spec.( like Rlim and so on), we can get the output current 12A based on our input voltage,

And please kindly advise how to calculate the max. output current thanks.

LM3150_EVOLUTION.pdf