Part Number: TPS546D24A
Hello,
I have two questions about TPS546D24A.
- The data sheet says in the Note of the section 7.5.2 Pin Strapping, "Allow a minimum 100 ms for the device to complete a burn of NVM User Store," but what's the maximum NVM programming time?
- Or, does it mean that the NVM programming will complete in 100 ms and it'll be no issue if a user waits for at least 100 ms?
- First, is it correct to understand that from the Table 7-14 of the data sheet there is no selection of the combination of "Auto Detect" for the "SYNC IN / SYNC OUT" and "32d – 47d" for the "SLAVE ADDRESS" range?
- Second, if that's correct, which SYNC direction, "Sync in" or "Sync out," do you recommend for a stand-alone (single-phase) device?
Best regards,
Shinichi Yokota