I want to use an external FET driver with the BQ27Z746 to achieve faster switching speeds than the internal charge pump would allow, but I still want to use the internal protection functions.
The CHG pin looks like it gets discharged to VSS (Vchgoff) and the DSG pins gets discharged to PACK (Vdsgoff).
Using the CHG pin as a logic input for the external FET driver looks like it should be simple (voltage divider to the correct logic level input of the driver).
But the DSG pin's low level is PACK. If I don't need the battery sensing buffer of the Zero-Volt charging mode, can I connect the PACK pin to VSS?