This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Recommended IC for dual battery charge with prioritised power path

Other Parts Discussed in Thread: BQ24617

I'm planning to design a portable device which has two 4S1P li-ion batteries, one of which is hot-swappable. The device will also feature a DC power input to charge both batteries, which should also power the device when plugged in. The power supplies should be prioritised ideally so that the hot swappable battery is used in preference to the other battery.

Can you help me select a suitable product for this?

Should I use two BQ24617 plus some sort of external power path selection logic? Or some other charger IC with some sort of smart features? Does TI offer a suitable IC?