Other Parts Discussed in Thread: LM3488, LM5155, LM5121
Hello support team,
I use LM3488 for conversion - from 12v to 24v.
(classical boost converter)
it should support up to 2.2A at the output (short pulse), for some worst case, but the planned average current consumption will not exceed 2A.
I tried practically the schematic , suggested by TI's tool WeBench, but I encountered in some issue - hard inrush current, at the beginning of the operation , which reaches 5A !
there is some "soft-start" feature already implemented in LM3488, I saw delay about 2ms - between rising of 12v at the input and start of DC/DC switching, generally this soft-start feature works, but it is not enough...
could you please suggest any additional solution/trick ?
(for example, I added capacitor 100nF in parallel with upper feedback resistor, it helps but partially)
the target is that the inrush current should not exceed 3A.
Thanks.