Hello,
I would like to use the buck 2 of the TPS650861 to generate the 0.85V core voltage (VCCINT) of a XCZU17EG (Zynq Ultra Scale +) taking the following points into consideration:
-> buck 2 controls a CSD87335 external FETs
-> Vout = 0.85V
-> Iout = 15A
-> expected accuracy is +-3%
The datasheet gives a +-2% accuracy for Iout up to 7A. Will the +-2% accuracy be respected at 15A ?
Can I use the buck 2 of the TPS650861 for this purpose ?
Thank you,
Regards.
Lionel