Hi Tech Support,
I am using the BQ27x10EVM. Is there any way that it can be configured such that on POR, NAC defaults to 100% of ILMD? The default for NAC on POR is 0, and I don't want to have to enter a "DONE" command every single time a new battery is put in. I am using primary batteries, so using the taper current settings isn't an option.
Any help would be much appreciated.
Thank you,
Christy
Cypress Envirosystems