This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92515HV-Q1: Output current overshoot and undershoot

Part Number: TPS92515HV-Q1


Hello,
It is found that the there is a significant overshoot and undershoot on output current when output LED voltage decrease or increase suddenly.
Attached waveform shows that the output current increase from 1.22A to 1.46A when output voltage decreases about 2.8V, and output current decrease from 1.22A to 780mA when output voltage increase about 2.8V.
So is there any proposal to decrease this overshoot and undershoot at ouput voltage transient?