Part Number: BQ24072
Other Parts Discussed in Thread: BQ24040
Hi there,
I am using your BQ24072RGTR battery charger. If i apply 4.73V in the input i get 0.47A on the battery side... with the same battery, if i apply 4.55V i get just 0.15A on the battery side (like if the maximum current is limited)... Is this an expected behaviour?? both voltages are within the bq operating conditions... i dont understand why the system is working differently...
Thank you so much.