Hi TI,
On a design of mine with the BQ2970, I've found that DOUT is sent low when a battery is first connected to my circuit. DOUT goes high as soon as the battery is connected to a charger and stays high even when the charger is removed, regardless of how long the battery was allowed to charge.
I am also noticing that the V- pin is being pulled up so that it is 1.2V less than the BAT pin. These behaviors seem to be consistent with the BQ2970's undervoltage protection. It seems that the UVP is being tripped erroneously because this happens even when a fully charged battery is plugged in. UVP should only be tripped when VBAT- VSS < 2.8V, but this should never be the case with a fully charged battery.
I am wondering if this has something to do with the battery being hot-plugged. Is there any way that I can just plug in a battery and have it work without needing to connect a charger to clear the UVP condition?
Thanks!