Hi,
We have the following questions regarding TPS65951:
1) How can we set the battery voltage threshold for the PMIC to power on the OMAP? The datasheet for the TSP65951 in table 6-24 talks about "main battery charged threshold" (VMBCH) which is fixed at 3.1V. Not sure if this is the turn-on voltage threshold. Is there any way we can change this?
2) Hands free speaker driver with stereo audio- can they mix to mono?
3) Do we need input and/or output caps for unused LDOs on PMIC?
Thanks,
Jeff