Based on the following description, can it be understood that the triggering conditions for the two low power modes are as follows
Is there a truth table for several modes?
Partial IO: PMIC_ ENABLE=0; PMIC_ Nsleep don't care
IO+DDR : PMIC_ ENABLE=1; PMIC_ Nsleep=0
Active:PMIC_ ENABLE=1; PMIC_ Nsleep=1
Are there power consumption tables corresponding to the two low power modes?