Other Parts Discussed in Thread: LM3463, LM3464
Hi,
I am going to use this part for only one LED string with 22 LEDs in series with maximum 82.5V, by respect the max input voltage 95V.
I have some questions:
1. If I only use one channel and do not use the rest (left open the 3 other channels) would that be any issue in this case?
2. What would be the efficiency?
3. Do you recommend this Part? It is apparently not new, and the chip is quite big!
4. Is there any alternative for this chip?
I found another part (LM3463) and it has 6 channels. Are the answer of above questions true for this part as well?