This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25576: Two LM25576 ICs synchronization

Part Number: LM25576


I want to operate two LM25576 integrated circuits as inverted buck boost and at the same time I want to synchronize them with each other. The synchronous pin is not included in the simulations. Can you help with this issue? Is there a reference source?

First LM25576 Vin 7v Vout -5V

Second LM25576 Vin 7v Vout -12v.

If you want I can share WEBENCH design.

Please help. Best Regards.