Other Parts Discussed in Thread: TPS61022, TPS61023
Hello,
Is there a specific reason for the 200uF maximum recommended output capacitance for the TPS61021A? Is it related to loop stability? In-rush? Or is it just a matter of adjusting the FF compensation capacitor and thus not truly a hard limit?
I am interested in driving a speaker (w/ Class D Amp) downstream from this output, with a 470uF electrolytic on the TPS61021A output rail due to high source impedance battery supply. So preferably I would place it at the output of TPS61021A instead of the input. Peak output current (non-inrush) from TPS61021A is likely about 1A and configured at 3.3V output.